AIN#.VALUE
Description
AIN#.VALUE reads the analog input value after the value is filtered (as shown in the Analog Input Block Diagram).
Examples
Code
--> AIN1.VALUE 1.420 V
Context
For more information see Analog Input.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read Only |
| Units | V |
| Range | -12.5V to +12.5V |
| Default Value | N/A |
| Data Type | Float |
| See Also | |
| Stored in Non Volatile Memory | No |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AIN1.VALUE | 0x3780 | 0x1 | INT | 1000:1 | - | RO | True |
| AIN2.VALUE | 0x3781 | 0x1 | INT | 1000:1 | - | RO | True |
|
Copyright © 2018 Kollmorgen |
|